;aiu; [Update] Name = LTspice 26.0.1 ProductVersion = 26.0.1.0 URL = https://LTspice.analog.com/download/26.0.1/LTspice64.msi Size = 178915328 ReleaseDate = 15/12/2025 SHA256 = EC35026697ED32D2AE57B17BE3A3C8877B631F642B66326491A9808C47EC0081 MD5 = ee98745ccbee42786343bd2cd2e93351 ServerFileName = LTspice64.msi Flags = Critical|Sys64|Os64 RegistryKey = HKUD\Software\Analog Devices Inc.\LTspice\Version Version = 26.0.1.0 UpdatedApplications = LTspice[1.0-26.1.0.3] DescriptionHtml = Update for LTspice: (Removes old installation to make use of new features) Description = Update for LTspice: (Removes old installation to make use of new features) FeatureHtml = What’s New in LTspice 26.0.0 Feature = What’s New in LTspice 26.0.0 Feature1 = Parallel release on MacOS and Windows Feature2 = • Add support for ARM processors Feature3 = • Improved convergence Feature4 = • Add support for loadstate/savestate/convreport defined as part of .tran analysis directive Feature5 = • When editing a schematic, automatically start wiring if an unconnected pin is left-clicked Feature6 = • Indicate default series resistance of 1mOhm when editing inductors on a schematic Feature7 = • - Remove Settings > Hacks > Always default inductors to Rser=0 Feature8 = • - To use default Rser=0 for all inductors, add ".options thev_induc=1" to the circuit Feature9 = • * Symbols autogenerated from .subckt's only include ModelFile base file name, not full path Feature10 = • Add schematic menu action Hierarchy > Generate Subckt Netlist Feature11 = • - Optionally use a symbol of the same name to define the subckt port order Feature12 = • Add unicode support for file paths in GUI menus/dialogs stored in .ini settings file Feature13 = • Improve display of recent files in File menu, show full path in status bar when hovered Feature14 = • Add log warning for extreme value capacitors (>1kF) regarding default parallel resistance Feature15 = • Change default value for waveform compression to disabled (Settings > Compression) FeatureHtml16 = What’s New in LTspice 24.1 Feature16 = What’s New in LTspice 24.1 Feature17 = • Added a SCOPEDATA choice to the voltage/current source dialog. The file name can now be a string parameter. Feature18 = • Improved performance and convergence Feature19 = • Behavioral source expressions using node voltages like "V(node)" can use a string parameter, e.g. "V({param})" Feature20 = • Relaxed netlist syntax requirements Feature21 = - Syntax errors inside unused sub-circuit definitions in libraries are silently ignored if they are not instantiated Feature22 = • MOS Model binning now silently ignored if only one model Feature23 = • Improved stepped trace behavior in waveform viewer Feature24 = • Improved Nyquist for Loop waveform representation behavior Feature25 = • Convergence optimizations Feature26 = • Add .savestate and .loadstate simulator directives to save and restore the complete transient simulation condition Feature27 = • Add .option debugtran to add report in log file to help identify convergence challenges Feature28 = • Enhanced netlist syntax checking Feature29 = • Changed default integration method to Trapezoidal Feature30 = • Remember waveform compression settings (under Settings > Compression) between LTspice invocations Feature31 = • Always accept “3k4” notation as 3.4k (no longer optional) Feature32 = • Allow device flags to be set to zero for ease of parameterization Feature33 = • Updated FRA example fra_eg1 Feature34 = • Updated Help documentation Feature35 = • Bug fixes FeatureHtml36 = What’s New in LTspice 24 Feature36 = What’s New in LTspice 24 Feature37 = We recommend that you update components after installing or updating LTspice. Feature38 = In LTspice, choose Tools > Update Components to install the latest LTspice library and models. FeatureHtml39 = Faster simulation speed and improved consistency Feature39 = Faster simulation speed and improved consistency FeatureHtml40 = UI Improvements Feature40 = UI Improvements Feature41 = • Icons and cursors have been updated Feature42 = • Default background has changed Feature43 = • Screen-resolution awareness scaling has been fixed Feature44 = • Default keyboard shortcuts have changed Feature45 = - Dynamic non-modal cheat sheet available from Help menu Feature46 = - Classic shortcuts still available via Feature47 = Edit Keyboard Shortcuts > Restore LTspice Classic Values FeatureHtml48 = Default trtol (time step control error tolerance) Feature48 = Default trtol (time step control error tolerance) Feature49 = changed to 2 for better performance in most applications FeatureHtml50 = Frequency Response Analysis (FRA) enhancements Feature50 = Frequency Response Analysis (FRA) enhancements Feature51 = • New 4-terminal probe Feature52 = - Enables analysis of uModules with integrated top feedback resistors Feature53 = - Simplifies analysis of inverting outputs and current feedback Feature54 = - Analyze any points in the loop Feature55 = • Plot phase margin (phase + 180) instead of phase Feature56 = • Smooth stimuli transitions for faster settling / improved accuracy Feature57 = ** Waveform viewer improvements Feature58 = • Rearrange plot panes via right-click > Move up/down, add above/below Feature59 = • Add menu items, shortcuts, and buttons to add/clear cursors Feature60 = • Annotate phase / gain margin via right-click > Notes Annotations Feature61 = • Annotate steps via right-click > Notes Annotations Feature62 = • Numerous bug fixes Feature63 = - Improved marching waveforms, including cursors and dragging traces FeatureHtml64 = Dialog improvements Feature64 = Dialog improvements Feature65 = • Better component selection Feature66 = - Cleaner, more intuitive layout Feature67 = - New quick links to analog.com product selector, and datasheets Feature68 = - Bug fixes Feature69 = • New subckt symbol parameter editor dialog FeatureHtml70 = New Configure Analysis toolbar button and shortcut ("a") Feature70 = New Configure Analysis toolbar button and shortcut ("a") Feature71 = • Tabs are populated with all possible simulation commands on the schematic Feature72 = • Edits to all tabs are mapped to schematic text Feature73 = • Schematic text is toggled between comment/directive appropriately FeatureHtml74 = Shift + Left-Click toggles between comment/directive Feature74 = Shift + Left-Click toggles between comment/directive FeatureHtml75 = Component libraries and AppData Feature75 = Component libraries and AppData Feature76 = • Faster, cleaner component updates Feature77 = - Libraries are cleaned up or overwritten on updates Feature78 = • Optional user-defined libraries for additional discrete components Feature79 = - By default, LTspice looks in Documents\LTspice for user.* Feature80 = (user.dio, mos, res, cap, ind, bead, jft, bjt) Feature81 = - Directory is configurable in Settings > Search Paths Feature82 = • Users should not edit ADI-provided files in %localappdata%\LTspice Feature83 = - LTspice will attempt to dissuade users from saving files here Feature84 = > Optionally share anonymous usage analytics to help us improve LTspice FeatureHtml85 = SPICE Log file improved and streamlined Feature85 = SPICE Log file improved and streamlined Feature86 = • Report LTspice version, non-default tolerances, etc FeatureHtml87 = Usability improvements, such as Feature87 = Usability improvements, such as Feature88 = • More items on Help menu, including Open Examples Feature89 = • New toolbar button to tile windows vertically Feature90 = • Settings dialog remembers last tab Feature91 = • Command line batch mode (-b) writes to stdout instead of showing GUI FeatureHtml92 = Numerous bug fixes Feature92 = Numerous bug fixes EnhancementHtml = 9/8/25 LTspice 24.1.10 Enhancement = 9/8/25 LTspice 24.1.10 Enhancement1 = • Improved step legend behavior in waveform viewer Enhancement2 = • Relaxed requirements for PWL files for independent sources Enhancement3 = - Automatically fall back to "PWL SCOPEDATA=..." behavior if the data is nonmonotonic. A warning is put in the log. Enhancement4 = • Added optional smoothed half-sine transition for pulse voltage sources EnhancementHtml5 = 5/26/25 LTspice 24.1.9 Enhancement5 = 5/26/25 LTspice 24.1.9 Enhancement6 = • .MEAS results saved into and SQLITE db file Enhancement7 = • Improved .savestate/.loadstate behavior when a capacitor value is changed between save/load Enhancement8 = • Changed FRA "Help me configure" wizard to always leave simultaneous harmonics blank (Nmax=1) EnhancementHtml9 = 5/2/25 LTspice 24.1.8 Enhancement9 = 5/2/25 LTspice 24.1.8 Enhancement10 = • Unknown .model parameters are now silent warnings again instead of errors Enhancement11 = • Attributes in schematic editor are only set to visible if they go from empty to populated (instead of any time they are changed) EnhancementHtml12 = 4/11/25 LTspice 24.1.7 Enhancement12 = 4/11/25 LTspice 24.1.7 Enhancement13 = • Nyquist for Loop representation added EnhancementHtml14 = 3/29/25 LTspice 24.1.6 Enhancement14 = 3/29/25 LTspice 24.1.6 Enhancement15 = • Enhanced table() function to load numbers from external file Enhancement16 = • Enhanced .wave directive EnhancementHtml17 = 3/09/25 LTspice 24.1.5 Enhancement17 = 3/09/25 LTspice 24.1.5 Enhancement18 = • Node names can be expressions again, this time officially documented and supported EnhancementHtml19 = 2/14/25 LTspice 24.1.3 Enhancement19 = 2/14/25 LTspice 24.1.3 Enhancement20 = • Re-enabled expanded netlist functionality EnhancementHtml21 = 2/1/25 LTspice 24.1.2 Enhancement21 = 2/1/25 LTspice 24.1.2 Enhancement22 = • Re-enabled caret operator Enhancement23 = • Duplicate .model cards are accepted if they are identical Enhancement24 = • Duplicate .func, .param, and .subckt are accepted if they come from the same location in the same file EnhancementHtml25 = 4/16/24 LTspice 24.0.12 Enhancement25 = 4/16/24 LTspice 24.0.12 Enhancement26 = • Default location for plot settings changed to schematic directory (instead of raw output directory) Enhancement27 = • Bring up Save As dialog when creating an auto-generated symbol from a netlist Enhancement28 = • Update FRA examples EnhancementHtml29 = 3/21/24 LTspice 24.0.10 Enhancement29 = 3/21/24 LTspice 24.0.10 Enhancement30 = • Improved font clarity in schematic text editor dialog Enhancement31 = • Bring up .step parameter editor when ".step temp ..." directive is right-clicked Enhancement32 = • Allowed placing .OP data labels at any time Enhancement33 = • Add working directory to top directory pull-down in Place Component dialog EnhancementHtml34 = 1/15/24 LTspice 24.0.7 Enhancement34 = 1/15/24 LTspice 24.0.7 Enhancement35 = • Right-click on symbol brings up attribute editor if model has multiple subckt's, to provide model selector pull-down EnhancementHtml36 = 1/8/24 LTspice 24.0.5 Enhancement36 = 1/8/24 LTspice 24.0.5 Enhancement37 = • Step Legend is now placed in plot rather than a modal window. Enhancement38 = • Enabled Text, Move, and Stretch toolbar buttons for the Waveform Viewer. Enhancement39 = • Added -version command line option. EnhancementHtml40 = 12/06/23 LTspice 24.0.3 Enhancement40 = 12/06/23 LTspice 24.0.3 Enhancement41 = • Command line batch mode (-b) writes to stdout instead of showing GUI BugFixHtml = 12/15/25 LTspice 26.0.1 BugFix = 12/15/25 LTspice 26.0.1 BugFix1 = • Bug fixes BugFixHtml2 = 12/1/25 LTspice 26.0.0 BugFix2 = 12/1/25 LTspice 26.0.0 BugFix3 = • Bug fixes BugFixHtml4 = 11/11/25 LTspice 24.1.10 BugFix4 = 11/11/25 LTspice 24.1.10 BugFix5 = • Bug fixes BugFixHtml6 = 5/28/25 LTspice 24.1.9 BugFix6 = 5/28/25 LTspice 24.1.9 BugFix7 = • Bug fixes BugFixHtml8 = 5/2/25 LTspice 24.1.8 BugFix8 = 5/2/25 LTspice 24.1.8 BugFix9 = • Bug fixes BugFixHtml10 = 4/11/25 LTspice 24.1.7 BugFix10 = 4/11/25 LTspice 24.1.7 BugFix11 = • Bug fixes BugFixHtml12 = 3/29/25 LTspice 24.1.6 BugFix12 = 3/29/25 LTspice 24.1.6 BugFix13 = • Bug fixes BugFixHtml14 = 3/09/25 LTspice 24.1.5 BugFix14 = 3/09/25 LTspice 24.1.5 BugFix15 = • Bug fixes BugFixHtml16 = 2/20/25 LTspice 24.1.4 BugFix16 = 2/20/25 LTspice 24.1.4 BugFix17 = • Bug fixes and minor improvements BugFixHtml18 = 2/14/25 LTspice 24.1.3 BugFix18 = 2/14/25 LTspice 24.1.3 BugFix19 = • Bug fixes BugFixHtml20 = 2/1/25 LTspice 24.1.2 BugFix20 = 2/1/25 LTspice 24.1.2 BugFix21 = • Other bugs fixed BugFixHtml22 = 1/25/25 LTspice 24.1.1 BugFix22 = 1/25/25 LTspice 24.1.1 BugFix23 = • Bug fixes BugFixHtml24 = 4/16/24 LTspice 24.0.12 BugFix24 = 4/16/24 LTspice 24.0.12 BugFix25 = • Fix rare waveform viewer crash BugFix26 = • Fix bug in schematic error misinterpreting simulation directives in certain situations BugFixHtml27 = 4/5/24 LTspice 24.0.11 BugFix27 = 4/5/24 LTspice 24.0.11 BugFix28 = • Fixed bug that caused problems with ascii data, plot settings, etc, in regions that use comma as decimal symbol BugFix29 = • Fixed bug that prevented automatic file extension concatenation in Save As function BugFixHtml30 = 3/21/24 LTspice 24.0.10 BugFix30 = 3/21/24 LTspice 24.0.10 BugFix31 = • Fixed -encrypt option in command line BugFixHtml32 = 2/2/24 LTspice 24.0.9 BugFix32 = 2/2/24 LTspice 24.0.9 BugFix33 = • Fixed broken link in the new ADI web page BugFixHtml34 = 1/23/24 LTspice 24.0.8 BugFix34 = 1/23/24 LTspice 24.0.8 BugFix35 = • Fixed a bug that caused noise analysis to get stuck if the schematic contained a syntax error BugFixHtml36 = 1/12/24 LTspice 24.0.6 BugFix36 = 1/12/24 LTspice 24.0.6 BugFix37 = • Fixed bug in pseudo-transient OP with .tran startup BugFix38 = • Renamed Step Legend as Annotate Steps and moved it's menu entry under ->Notes Annotations as well as Plot Settings->Notes Annotations BugFix39 = • Addressed high Ua values on the ISO16750 12V and 24V Load Dump Test A and B pulses BugFixHtml40 = 1/8/24 LTspice 24.0.5 BugFix40 = 1/8/24 LTspice 24.0.5 BugFix41 = • Fixed a bug concerning controlled source with POLY(n) syntax using parameters BugFixHtml42 = 12/13/23 LTspice 24.0.4 BugFix42 = 12/13/23 LTspice 24.0.4 BugFix43 = • Fixed a crash for netlists that contain only single-threaded devices BugFixHtml44 = 12/06/23 LTspice 24.0.3 BugFix44 = 12/06/23 LTspice 24.0.3 BugFix45 = • Minor bugs fixed BugFixHtml46 = 11/20/23 LTspice 24.0.2 BugFix46 = 11/20/23 LTspice 24.0.2 BugFix47 = • Minor bugs fixed BugFixHtml48 = 11/02/23 LTspice 24.0.1 BugFix48 = 11/02/23 LTspice 24.0.1 BugFix49 = • Minor bugs fixed AutoCloseApplication = [APPDIR]LTspice.exe